Issue:
Mounting method for Square D/Schneider Electric Sealed Resin Epoxy Encapsulated Transformers
Product Line:
LV Transformers
Environment:
Applies to Sealed Resin Epoxy Encapsulated Transformers ONLY
Cause:
Square D/Schneider Electric Sealed Resin Epoxy Encapsulated Transformers can be mounted differently from Ventilated or Non-Ventilated Transformers
Resolution:
Wall mounting is the standard mounting method for all Square D by Schneider Electric Sealed Resin Epoxy Encapsulated Transformers in style A, B, or C enclosures.
Publicado para: Schneider Electric Mexico