¿Cómo podemos ayudarte hoy?

Which of the Low Voltage Dry Type Distribution Transformers offered by SquareD/Schneider Electric are marked for use in Canada?

Issue:
Transformers for use in Canada

Product Line:
LV Transformers

Environment:
Applies to Low Voltage Transformers by SquareD/Schneider Electric

Cause:
Use of Low Voltage Transformers in multiple countries

Resolution:

SquareD/Schneider Electric`s Epoxy Resin Encapsulated Low Voltage Dry Type Distribution Transformers in enclosure styles A, B, C, or D are cULus labeled. cULus means that the unit is listed and labeled for both the UL and CSA standards.  Our 9070 T and TF Industrial Control Transformers are CE marked and 50 Hz and 60 Hz rated for use in many countries.  Single Phase EE type Energy Efficient Transformers also have the cULus symbol on the nameplate, making them suitable for use in Canada.


CTA-ID : 2007780

Schneider Electric Mexico

Documentos adjuntos
Resin White Book.pdf [832.93 KB]