¿Cómo podemos ayudarte hoy?

What color of paint does Square D used for the low voltage dry type distribution transformers? Is touch up paint available?

Issue:
Need the color and available part number for the paint used on Square D Low Voltage Transfomers.

Product line:
LV Transformers

Environment:
Low Voltage Transformers

Resolution:
The paint color is ANSI 49 gray. Touch up paint is available in an aerosol can and can be ordered with catalog number PK49SP. Since it is in an aerosol can, it CANNOT be shipped by Air. Rather it must go via ground.