¿Cómo podemos ayudarte hoy?

What is necessary to put a NQOD430L225 MLO interior in a MH44 or MH44WP?

Issue:
How to install NQOD430L225 MLO interior in a MH44 or MH44WP

Product Line:
NQOD panelboard

Environment:
Installation

Resolution:
The following parts will be required per panel:

(1) 80110-288-04 12`` rail extensions
(1) 80110-291-04 12`` MLO deadfront extension
(2) 80110-289-01 Deadfront mounting brackets
(2) 80025-067-01 Deadfront screws
(4) 21590-17081 Rail extension screws

Revised 3/10/04




CTA-ID : 2010258