¿Cómo podemos ayudarte hoy?

What does "Duty cycle tested minimum 5000 cycles" mean?

Issue:
What does "Duty cycle tested minimum 5000 cycles" mean?

Product Line:
TVSS Units

Environment:
Maintenance

Cause:
Replacement

Resolution:

The product undergoes testing for 5000 cycles in accordance with IEEE test standards, which specify a maximum current of 10KA and 20KV. It must successfully complete these test cycles with no more than a 10% degradation in its clamping voltage capability. Our products surpass these standard requirements.