What main breaker kit can be used with QBL, QDL, QGL, QJL or K frame for a 250 amp rating for an NQOD panel?
Main breaker kit used with QBL, QDL, QGL, QJL or K frame for a 250 amp rating for an NQOD panel
Product Line:
NQOD panelboards
Environment:
Installation / Setup
Resolution:
QBL, QDL, QGL and QJL breakers are 225A maximum. If a 250A main breaker is required, the panel must be factory assembled.