¿Cómo podemos ayudarte hoy?

Can the PTQ4680GH plug-in unit be installed on the busway while the busway is energized?

Issue:
Installing a PTQ4680GH plug-in unit on the busway  while the busway is energized

Product Line:
LV Busway.

Environment:
Products sold in North America

Cause:
Installation.

Resolution:
The customer should always follow the installation instructions that are provided with each of the plug-in units.
The warnings and instructions are different for each plug-in unit.