¿Cómo podemos ayudarte hoy?

Are NF panelboards available in Nema 12 enclosures?

Issue:
Are NF panelboards available in Nema 12 enclosures?

Product Line:
PTFDS - FD Enclosure System

Environment:
NF panelboard sold and supported in the USA.

Cause:
Selection of enclosures for the NF panelboard.

Resolution:
Yes. Refer to the current  Digest for selection.