¿Cómo podemos ayudarte hoy?

Can a 2-pole breaker serve as a disconnect for an SDSA1175 while also feeding a load?

Product Line:
Surge Protective Devices (SPDs)

Environment:
SDSA

Cause:
Application

Resolution:
Yes, only 15 or 20 ampere breakers can be used. However, there may be limitations on the quantity and size of conductors that can be terminated to the breaker.