¿Cómo podemos ayudarte hoy?

Do subfeed breakers use up pole spaces of the panel interior?

Issue:
Do subfeed breakers take up panel interior space or are they mounted separately?

Product Line:
NQ NF Panelboards

Environment:
Products sold in North America

Resolution:
The subfeed breakers are mounted within the box but below the standard interior branch spaces.  They do not use up the normal interior branch space.

Subfeed circuits do count toward circuits in the panel. So if you have a panel that must meet the 42 circuit rule then (2), 3 pole sub-feed breakers would count as part of the 42 circuits regardless if they take up space in the interior.

Schneider Electric Mexico

Explora más
Rango:
Categoría:
Explora más
Rango:
Categoría: