What is the part number of the red & black knob on the operating handle mechanism of a Model 5 LVMCC unit?
Red & black knob on the operating handle mechanism of a Model 5 LVMCC unit
Product Line:
Model 5 Motor Control Centers
Environment:
Products sold and used in North America
Cause:
Product features
Resolution:
40555-015-01 Red knob
40555-015-02 Black knob
The rivet that was used to attach the knobs has been obsoleted. To attach the knobs, use a long screw that can go through the knobs, and lock it with a knut on the other side.