¿Cómo podemos ayudarte hoy?

What is the hole diameter dimension for the lower mounting foot on the HC2674WP weatherproof box?

Issue:
Hole diameter dimension for the lower mounting foot on the HC2674WP box

Product Line:
I-line panelboards

Environment:
NEMA 3R Enclosure

Cause:
Product features

Resolution:
It is 1/2`` diameter.