Nuestras marcas

Bienvenido(a) al sitio web para México de Schneider Electric

Te damos la bienvenida a nuestro sitio web para México.
		
¿Cómo podemos ayudarte hoy?
Need details on the key locks for the HVL switch.
Issue:
Details on the key locks for the HVL switch.

Product Line:
Medium voltage switchgear.

Environment:
Products sold in the United States.

Cause:
Product features.

Resolution:
The standard OTM mechanism HVL switch has knockouts for 2 key locks below the switch handle and on the fuse door. There is a knockout for 1 key lock above the handle. The standard key lock is the Schneider Canada lock. All locks have 0`` bolt projection with the lock in the withdrawn position. ABB Kirk's key locks are interchangeable. Schneider locks are Type VFL for the switch and Type VDL for fuse door. ABB Kirk locks are Type KFL for the switch and Type KDL for fuse door.