¿Cómo podemos ayudarte hoy?

Does SquareD/Schneider Electric offer any fuse block opitons for the 9070 Type EO Industrial Control Transformer line?

Issue:
Fuse block options for EO Transformers

Product Line:
LV Transformers

Environment:
Applies to Industrial Control Transformers by SquareD/Schneider Electric

Cause:
Industrial Control Transformers may require fuse blocks

Resolution:

No primary fuse block option is available for the 9070 Type EO.  The secondary fusing options use a glass type fuse, 30 amps maximum.
The 9070AP3 is for the 25-150VA range.  The 9070AP4 is for the 200-750VA range.

The 9070 Type T has a complete line of fuse block options.


CTA-ID : 2010098