¿Cómo podemos ayudarte hoy?

What is the ambient temperature rating for 800A to 5000A copper and aluminum busway?

Issue:
Temperature rating for busway

Product Line:
I-Line Busway

Environment:
Products sold and used in North America

Resolution:
I-Line II busway is allowed to be operated in an ambient temperature range from -30 Degree C to +40 Degree C.