¿Cómo podemos ayudarte hoy?

What is the temperature rise rating of the Mini-Power Zone units?

Issue:
Listing of temperature rise for MPZ Transformers

Product Line:
LV Transformers

Environment:
Applies to Mini-Power Zone Transformer Units by SquareD/Schneider Electric

Cause:
Transformer construction typically offers 150C, 115C and 80C temperature rise options

Resolution:

Standard MPZ units are rated for a 115 Degree C maximum temperature rise.  An 80 Degree C rise option is available on certain models.