¿Cómo podemos ayudarte hoy?

Can the NEMA 1 NQ panelboard be flush mounted?

Issue:
Flush mounting NQ panelboards.

Product Line:
Panelboards.

Environment:
Products sold in North America

Resolution:
Yes, the NQ NEMA 1 panels can be either surface mounted or flush mounted. Order the flush cover in order to mount the box flush inside the wall.