¿Cómo podemos ayudarte hoy?

Video: What is a finger safe cover for a 9070 Type T Industrial Control Transformer with either factory installed (type TF) or field installed 9070FB(2A,2B,3A, or 3B) fuse block?

Issue:
What is the part number for finger safe covers for 9070 CPT's?

Product Line:
Industrial Control Transformers

Environment:
9070T 9070TF

Resolution:
The installation of the 9070FP-1 fuse puller kit may help comply with CE specifications regarding finger safe protection.  The kit includes three fuse pullers, one for each pole of the standard 3 pole fuse block.