What are the mounting provisions for a 200 ampere circuit breaker bucket, catalog number 8998HBF200, for a Model 6 Motor Control Center?
200 ampere circuit breaker bucket mounting provisions, catalog number 8998HBF200 for a Model 6 MCC.
Product Line:
Motor Control Center 6
Environment:
North America Product
Cause:
N/A
Resolution:
In order to install the 6`` Compact bucket with a 200A breaker, the installer must allot 6`` of vertical mounting space for it, and also must remove a section of vertical wire trough to obtain proper wire bending space.