¿Cómo podemos ayudarte hoy?

Are Split Bus NQ Panelboards Available?

Issue:
Are NQ panels available with split bus configurations?

Product Line:
NQ Panelboards

Environment:
Application

Cause:
Product Selection

Resolution:
The NQ panelboard product line has a standardized Split Bus offering:
1) Main 18ckts - Split 30ckts
2) Main 30 ckts -Split 18 ckts
3) Main 30ckts and Split 30 ckts
The NQ Split buss Panels are offered up to 225A Maximum , using Engineering Product selectors , that can be quoted from either a Distributor , or the SQ D/ SE Sales Office.