¿Cómo podemos ayudarte hoy?

How many blank fillers are provided with merchandised, RTI, NQ panelboard interiors?

Issue:
Are blank fillers provided with merchandised, RTI, NQ panelboard interiors?

Product Line:
Low Voltage Panelboards

Environment:
NQ Panelboards

Cause:
Product Features

Resolution:
A bag of 15 one pole blank fillers is supplied with NQ interiors with 18, 30 and 42 circuits. Two bags, a total of 30, of one pole blank fillers is supplied with 72 and 84 circuit interiors.