¿Cómo podemos ayudarte hoy?

Is the 42 circuit NQ panelboard interior able to be retrofitted into an existing MH35 box?

Issue:
Can the 42 circuit NQ panelboard interior be field installed into an existing MH35 box?

Product Line:
NQ Panelboards

Environment:
Maintenance/installation/retrofit

Resolution:
No, customer will need to replace with current NQ option.