¿Cómo podemos ayudarte hoy?

What is the catalog number for the fasteners used on the front covers/buckets of a Model 4 Motor Control Center?

Issue:
Catalog number for the fasteners used on the front covers/buckets of a Model 4 Motor Control Center

Product Line:
Model 4 motor control center.

Environment:
Products sold in the United States.

Cause:
Maintenance.

Resolution:
The catalog number is 3031715301 for the thumbscrew used on covers/doors/buckets. Catalog number 2350220003 is the captive cage nut installed on the frame (which the thumbscrew screws into to hold the cover/door in).