¿Cómo podemos ayudarte hoy?

What are the dimensions on catalog number NC44FHR?

Issue:
What are the dimensions of the NC44FHR hinged panel cover?

Product Line:
NF Panelboards and Accessories

Environment:
NQ and NF panelboard covers

Cause:
Product Features

Resolution:
The height on the panelboard cover is 45.52`` and the width is 21.52``.