¿Cómo podemos ayudarte hoy?

What is the difference between the two Transformers with catalog numbers 15T2FSS and 4X15T2FSS?

Issue:
Stainless Steel Transformer enclosures

Product Line:
LV Transformers

Environment:
Applies to Epoxy Resin Encapsulated Transformers by SquareD/Schneider Electric

Cause:
There is a difference between Stainless Steel Transformer enclosure NEMA ratings

Resolution:
15T2FSS is Nema 3R stainless steel enclosed transformer and 4X15T2FSS is Nema 4X stainless steel enclosed transformer - both are three phase,15kVA, 480V Delta primary to 208Y/120V secondary.