¿Cómo podemos ayudarte hoy?

Is a drip shield available to convert a box HC2665B to be rated at NEMA 2 rather than NEMA 1?

Issue:
Is a drip shield available to convert a box HC2665B to be rated at NEMA 2 rather than NEMA 1?

Product Line:
Panelboards.

Environment:
I-Line

Cause:
Availability.

Resolution:
The sprinkler proof endwall is catalog number HCT2DH26. This is a Type 2 Driphood, mostly used in Canada.


CTA-ID : 2046320