¿Cómo podemos ayudarte hoy?

What are the input and output voltages for the CE marked S67 Transformers?

Issue:
Export Model Epoxy Resin Encapsulated Transformers

Product Line:
LV Transformers

Environment:
Applies to Low Voltage Transformers by SquareD/Schneider Electric

Cause:
Transformers with non-Domestic or European Voltages

Resolution:
Primary 190/200/208/220 x 380/400/416/440
Secondary 110/220 50/60 hertz
cULus Listed and CE marked for import into the European Union


CTA-ID : 2045531