¿Cómo podemos ayudarte hoy?

What is the replacement for a QMB3610T Series 1-4 QMB switch?

Issue:
What is the replacement for a QMB3610T QMB switch?

Product Line:
QMB panelboards sold and supported in tNorth America

Environment:
Cross reference, replacement.

Cause:
Replacement for obsolete QMB3610T.

Resolution:
If the QMB panel board was built before 1961, there is no viable replacement.
If the QMB panel board after 1961, but before 1984, a QMB363T, Series D2, QMB switch may be a suitable replacement. The QMB363T requires 7.5" of panel mounting space and may require a QMB310EX Plug-On Extension Assembly if the existing panel is a 38" wide QW panel board or a free standing switchboard.