¿Cómo podemos ayudarte hoy?

What are the rail extensions for the NQ panels?

Issue:
Are there an available rail extensions for the NQ panelboard?

Product Line:
NQ Panelboards

Environment:
For use on Main Lugs Panelboards only (not for use on Main Breaker Panelboards). UL 67, UL 50, CSA C22.2 No.'s 20-M1989 & 94-M91, NEMA PB1, NFPA 70 Art. 408, Federal Specification W-P-115C Type 1 Class 1 , 2003 IBC, NFPA

Cause:
Application of rail extensions.

Resolution:
The following are the rail extensions for NQ panelboard. They are for use only on Main Lugs Panelboards (not Main Breaker Panelboards).

6 inch rail and deadfront extension: NQ6RDE
12 inch rail and deadfront rail extension: NQ12RDE
18 inch rail and deadfront rail extension: NQ18RDE
24 inch rail and deadfront rail extension: NQ24RDE