¿Cómo podemos ayudarte hoy?

Is there any restrictions with mounting a QO2125 or QOB2125 into an NQ interior?

Issue:
Restrictions mounting a QO2125 or QOB2125 into an NQ interior

Product Line:
Panelboards.

Environment:
Products sold in the United States.

Cause:
Product features.

Resolution:
There is a 40A maximum mounted across from a 125A branch breaker. Space the circuits accordingly.


CTA-ID : 2047311