What is the part# for the main lug and lug mounting screw for NF 125A or 250A main lug interior?
Part number for the main lug and lug mounting screw for an NF 125A or 250A main lug interior
Product Line:
NF panelboards and accessories
Environment:
Maintenance/Replacement
Cause:
Replacement main lug
Resolution:
One main lug was part# 80114-031-01, which is obsolete replaced by a 80114-312-50. The lug mounting screw is part# 80114-001-01. Two screws required per lug.
CTA-ID : 2048742