¿Cómo podemos ayudarte hoy?

Can NF 600A Main breaker panelboards be engineered to have a 84 circuit double tub configuration?

Issue:
NF 600A Main breaker panelboards with 84 circuit double tub configuration

Product Line:
Panelboards.

Environment:
Products sold in the United States.

Cause:
Product features.

Resolution:
No, because the LC main breaker is used for 600A factory assembled panel. This restricts the selection of a 84 circuit, double tub panel. A double panel can be entered onto product selectors as 2 separate line items. The first section has the main breaker and feed-thru-lugs. The second section is a main lug only interior. Note that the box sizes will be different.


CTA-ID : 2048402