¿Cómo podemos ayudarte hoy?

Will older style (pre-1986) QOB branch breakers fit into the NQOD or NQ Panelboards?

Issue:
Fitting Older QOB branch breakers into the NQOD or NQ Panelboards

Product Line:
Circuit Breakers and Panelboards

Environment:
Applies to QOB Breakers, NQOB, NQOD, and NQ Panelboards

Resolution:
QOB circuit breaker have been manufactured since the 1950's. Sometime around 1986, the QOB circuit breakers were given a new bolt-on connector. This design change did not affect their use in NQOB panels. However, the NQOD and NQ Panelboards will not accept the older design connector that was on the pre-1986 QOB breakers. There is no problem using the new bolt-on connector QOB breakers in NQOD and NQ Panelboards. See the below pictures showing the pre-1986 connector and the post-1986 connector.

QOB pre-1986 connector
qob

QOB post-1986 connector
qob


Schneider Electric Mexico

Explora más
Rango:
Categoría:
Explora más
Rango:
Categoría: