What is the life expectancy of the 9070T and 9070TF Industrial Control Transformers?
Issue:
Life expectancy for T and TF style Industrial Control Transformers
Product Line:
LV Transformers
Environment:
Applies to Industrial Control Transformers by SquareD/Schneider Electric
Cause:
Applications frequently require lifetime estimates of Industrial Control Transformers
Resolution:
The published mean life of the insulation system is 10,000 hours under normal operating conditions.
This value is impacted by loading and ambient conditions and precludes mechanical effects or circuit anomalies.
Publicado para: Schneider Electric Mexico