What is the largest branch breaker available in the 400A NQ panel in a NEMA 3R enclosure?
Issue:
What is the maximum amp of a branch breaker that can be installed in a 400A NQ panel in a weatherproof enclosure?
Product Line:
NQ Circuit Breaker panels sold and supported in the USA.
Environment:
Specifications
Cause:
Product Features
Resolution:
Four (4) 150, 175, or 200 A QO(VH) plug-on branch circuit breaker may be installed in 8.75 in. deep MHxxD9VWP NEMA 3R enclosures.
What is the maximum amp of a branch breaker that can be installed in a 400A NQ panel in a weatherproof enclosure?
Product Line:
NQ Circuit Breaker panels sold and supported in the USA.
Environment:
Specifications
Cause:
Product Features
Resolution:
Four (4) 150, 175, or 200 A QO(VH) plug-on branch circuit breaker may be installed in 8.75 in. deep MHxxD9VWP NEMA 3R enclosures.