¿Cómo podemos ayudarte hoy?

Can a J Frame breaker with a Motor Operator be installed in an I-Line panelboard?

Issue:
Installing J Frame breaker with a Motor Operator on an I-Line panelboard

Product Line:
I Line Panelboard

Environment:
Accessory

Cause:
Installation clarification

Resolution:
Yes, in I-Line panels that will accept J Frame breakers. However, the Motor Operator mandates use of a 4 piece trim with NO door option, since a door will not close over a motor operator.