¿Cómo podemos ayudarte hoy?

Can the ATV61 or ATV71 keypad be used in direct sunlight with remote mount kit VW3A1102 or VW3A1103?

Issue:
Can the ATV61 or ATV71 keypad be used in direct sunlight with remote mount kit VW3A1102 or VW3A1103?

Product Line:
ATV61 ATV71

Environment:
All

Cause:
Remote keypad in direct sunlight

Resolution:
No. The display cover is not UV protected. The display will not function properly if exposed to direct sunlight over time.