¿Cómo podemos ayudarte hoy?

Does a RSV Trench Duct come with couplings?

Issue:
Are couplings included in RSV Trench Duct?

Product Line:
Trench Duct

Environment:
RSV Square D Trench Duct

Resolution:
Yes as standard. Each Trench Duct straight length comes with 2) aligning keys (couplers).The part number for the alignment key assembly is 45206-176-50.