¿Cómo podemos ayudarte hoy?

Can an H frame breaker with a motor operator be installed in an I-Line panelboard?

Issue:
Install an H frame breaker with a motor operator in an I-Line panelboard

Product Line:
I line panelboards.

Environment:
Products sold and used in North America

Cause:
Product features.

Resolution:
Yes. However, this can only be done in NEMA 1 enclosures with a 4 piece trim. It cannot be done in applications that require a door.