Are the NQ and NF panelboards UL50 and UL67 rated?
Do NQ or NF panelboards meet the both UL50 and UL 67 requirements?
Product Line:
Panelboards.
Environment:
NQ and NF Panelboards
Resolution:
Yes. Both UL50 and UL 67 requirements are met for NQ and NF panelboards.