What do you get when you order a SK5668 kit?
What is included in the SK5668 bus finger kit fro NQOB panelboards?
Product line:
Obsolete panelboards
Environment:
NQOB panelboard accessories
Resolution:
This is a horizontal bus bar kit for NQOB panels to convert to QOB breakers in lieu of Q1B style. The connectors cannot be ordered separately. Each kit contains:
(3) A & C phase connectors
(3) A & C connector screws
(2) B phase threaded screw
Revision 04/10
Note: An SK5668, has enough bus connector parts to add 6 pole spaces on a single or 3 phase NQOB panelboard. If for single phase, this is qty 6 single poles or qty 2 of 2 pole plus qty 2 of 1 pole breakers. Cannot install qty 3 of 2 poles in the single phase panelboard.