¿Cómo podemos ayudarte hoy?

What are the part numbers for the optional fan kit for the Altistart 22 soft starter?

Issue:
Part numbers for the optional fan kit for the Altistart 22

Product Line:
ATS22

Environment:
All serial numbers for ATS22

Cause:
N/A

Resolution:
The ATS22 'S6" version utilizes 230V fans.
The ATS22 'S6U" version utilizes 120V fans.

ATS22D17..., D32, and D47 = VW3G22400 (230V) or VW3G22U400 (120V)
ATS22D62..., D75, and D88 = VW3G22401 (230V) or VW3G22U401 (120V)
ATS22C11..., C14, and C17 = VW3G22402 (230V or VW3G22U402 (120V)

This is an optional external fan that mounts to the back of the ATS22 and has a plug that attaches to the bottom of the ATS22.

ATS22 fan kits

See the ATS22 User Manual starting on page 20 for more details.