¿Cómo podemos ayudarte hoy?

What is the heat loss in BTU`s for a Panelboard?

Issue:
What is the heat loss in BTUs for a circuit breaker panelboard?

Product Line:
Circuit Breaker panelboards

Environment:
Heat loss

Resolution:
3.25 BTU/ minute no matter what the load or panelboard type. This converts to 819 calories per minute.
In addition, you have to add in the contribution of each breaker installed.