¿Cómo podemos ayudarte hoy?

What is the maximum distance for 225A Powerbus busway run?

Issue:
Powerbus max distance

Product Line:
Powerbus 225 Busway

Environment:
Products sold in North America

Cause:
Voltage drop

Resolution:
There is no maximum distance restrictions using the 225 amp Powerbus busway.
Note:  Powerbus does have a 2.5Volt drop per every 100 feet.This is based on 100% power factor (Pf).