¿Cómo podemos ayudarte hoy?

How is the ATV12 programmed for a 0-10Vdc analog input on AI1?

Issue:
Programming an ATV12 for a 0-10Vdc analog input on AI1

Product Line:
ATV12

Environment:
Programming

Cause:
n/a

Resolution:
The factory default is for a 0-5Vdc input.  Set AI1t = 10U to accommodate a 0-10V input.  AI1t is found in the IO menu and AI1 submenu.