Is there a table in Proworx that indicates what number equates to the EMTH block ?
No. The table below indicates the reference number for the desired EMTH block.
| Reference Number | EMTH Function |
| 1 | ADDDP |
| 2 | SUBDP |
| 3 | MULDP |
| 4 | DIVDP |
| 5 | SQRT |
| 6 | SQRTP |
| 7 | LOG |
| 8 | ANLOG |
| 9 | CNVIF |
| 10 | ADDIF |
| 11 | SUBIF |
| 12 | MULIF |
| 13 | DIVIF |
| 14 | SUBFI |
| 15 | DIVFI |
| 16 | CMPIF |
| 17 | CNVFI |
| 18 | ADDFP |
| 19 | SUBFP |
| 20 | MULFP |
| 21 | DIVFP |
| 22 | CMPFP |
| 23 | SQRFP |
| 24 | CHSIN |
| 25 | PI |
| 26 | SINE |
| 27 | COS |
| 28 | TAN |
| 29 | ARSIN |
| 30 | ARCOS |
| 31 | ARTAN |
| 32 | CNVRD |
| 33 | CNVDR |
| 34 | POW |
| 35 | EXP |
| 36 | LNFP |
| 37 | LOGFP |
| 38 | ERLOG |