What Schneider devices will connect using the (TCSMCNAM3M002P) USB to RS485 converter?
The TCSMCNAM3M002P is compatible with the following device families (RJ45 socket):
Advantys OTB
Altistart Series
Altivar series incl. HMI
Altivar Controller inside,
SD3 28 Stepper Drive
Lexium Motion Controller
Lexium Servo Drives
Magelis XBT N/R/RT
M238 and M340 Controller,
TesysU / TesysT System
XPS MC Safety Controller
Note: TCSMCNAM3M002P is NOT compatible with Modicon Quantum and Modicon Momentum. Due to a different connector pinout.
Legacy KB System (APS) Data: RESL201395 V1.0, Originally authored by GeMc on 02/19/2010, Last Edited by GeMc on 02/19/2010
Related ranges: Magelis XBT N, R, RT, Modicon M340
Publicado para: Schneider Electric Mexico