¿Cómo podemos ayudarte hoy?

What is the default TCP port number of the native Ethernet Port on M340 BMXP342020 processor.

Product:

M340

Answer:

The proprietary TCP port number for Modbus/TCP traffic for the M340 BMXP342020 processor's native ethernet port is 502.