Part number for the fiber cable used between the Primary and Standby CPU's in a Unity (CE14) Hot Standby application and Is this cable included in my purchase of the 140CPU671 60?
This cable is not included in your purchase of the 140CPU671 60. The part number(s) of the fiber MT/RJ cable are:
490NOR0003 3 m MTRJ/ MTRJ
490NOR0005 5 m MTRJ/ MTRJ
490NOR0015 15 m MTRJ/ MTRJ
Publicado para: Schneider Electric Mexico