¿Cómo podemos ayudarte hoy?

Can the CHS module in a Quantum Hot Standby system be 'Hot Swapped'?

No. The CHS module will not link up with the PLC if it is hot swapped'. If the CHS was hot swapped a re-boot of the CPS power supply is necessary for recovery.